AnsweredAssumed Answered

AD-FREQCVT1 With FMCOMMS5

Question asked by ttyler777 on Feb 7, 2017
Latest reply on Feb 9, 2017 by mhennerich

Hello,

 

I am looking for some help getting a AD-FREQCVT1 to work with my FMCOMMS5.  I'm following this guide (https://wiki.analog.com/resources/eval/user-guides/ad-freqcvt1-ebz), but when I get to the software section, it says to check a box that does not exist on the FMCOMMS5 tab.  What steps are required to get the FMCOMMS5 to work with the AD-FREQCVT1?  I'm using a ZC706 dev board.

 

Tyler Jackson

 

EDIT:

Here's some more info that I neglected to mention:

 

I'm on a Windows 7 64-bit machine.

 

I was able to connect power cable to the FMCOMMS5 board and then connect the data cable to the ZC706 board.  I can't tell if it's working however, since I don't have the device listed under my /sys/bus/iio/devices/ directory.  Do I need to load a different devicetree into the image?  I'm currently using the "zynq-zc706-adv7511-ad9361-fmcomms5" file when I build my image.

Outcomes