AnsweredAssumed Answered

COULD NOT CONNECT TO IIO server

Question asked by wills on Feb 6, 2017
Latest reply on Feb 12, 2017 by rejeesh

Dear Di,

I have strictly followed the the download instructions on the page and fixed one of the issues ..its now see the header files.

 

The new error in both cases ie MATLAB/SIMULINK is:

 

“ COULD NOT CONNECT TO IIO server ”

 

 

Take a look, though the script is for ad9361; I changed the s.dev_name = ’ad9364’

since my device is AD-FMCOMMS4-EBZ

 

BUT

You can see after line 12, that the S (system object) did not return the cell array expected  but -1  => S is destroyed  and it stops execution at line 14 ..

 

 

 

COULD IT BE BECAUSE THE HARDWARE IS NOT YET CONNECTED TO MY LAPTOP?

 

Find attached the two instaces

 

Regards

 

-Wills

Attachments

Outcomes