AnsweredAssumed Answered

AD9371 Rx EVM related

Question asked by nagnerella on Feb 3, 2017
Latest reply on Feb 8, 2017 by Vinod

Hi

I have following questions on AD9371.

 

  1. Based on datasheet AD9371 Datasheet at 2600MHz shows as below. This is with what gain in AD9371? If AGC is enabled what is the target gain backoff condition? Is it 15dB?

2. For a case where my LTE system has the same signal level of input for both interference and the operating channel. Assume here both of them are LTE signals. Do you have the Rx EVM numbers under this scenario.

Based on datasheet i realize noise figure data only mentioned. Do you have the data of  RX EVM with interferer level.

Regards

Nagaraju

Outcomes