AnsweredAssumed Answered

    ZC706-FMCOMMS5 hdmi is not booting from linux image

Question asked by SuDhaMani on Feb 3, 2017
Latest reply on Feb 10, 2017 by larsc

Hi

 

I am working on ZC706 with add on FMCOMMS5 analog board. I am using the SD card image taken from (Zynq & Altera SoC Quick Start Guide [Analog Devices Wiki] -23 December 2016 release (2016_R1) ) . I have followed proper procedure as mentioned to copy boot files into the base directory. I am monitoring through serial port. The log is attached here. I can see DONE led going high,but HDMI monitor is not displaying anything. In the log i can see it is getting struck at "VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2): error -30". Any help would be appreciated.

 

zc706 ad-fmcomms5 cf_adv7511_zc706 ad-9361 driver linux adi iio oscilloscope

 

Thank you

Attachments

Outcomes