AnsweredAssumed Answered

ADV7619->ADV8005

Question asked by qwerty78 on Jan 31, 2017
Latest reply on Mar 27, 2017 by mattp

I'm trying to bring up a board with an ADV7619 to ADV8005 through the TTL input pins.

 

My computer detects the board and is sending video at 1080p60. The  ADV7619 has a TMDS lock with a measured pixel clock of ~138 MHz and is set to output a 36-bit 4:4:4 SDR bus.

 

I'm having difficulty getting the ADV8005 to detect the VIC and output a proper video.  I have the EVAL-ADV8005, but since it uses the serial input, I haven't been able to test my scripts on the ADV8005 for TTL input.

 

I've attached my configuration script.  Is there something that I'm missing?

 

Also, is there way to configure the EVAL-ADV8005 to use the 7842 and the TTL inputs of the 8005?  When I've tried it, my computer does not detect the eval board.

Attachments

Outcomes