AnsweredAssumed Answered

Monitor the received signal level or SNR with the EK1HMC6350 eva-kit?

Question asked by bhan on Jan 31, 2017
Latest reply on Feb 10, 2017 by Mark_D

Hi,

 

I'm considering about setting up a simple 60GHz channel measurement system with the EK1HMC6350 Eva Kit, and I am wondering if there is any chance that I monitor the SNR or received signal level without applying an extra oscilloscope/spectrum analyzer?

 

If yes, in the RF band or the base band? If not, or if only in the base band, is there an AGC in the analog signal chain which I am not able to know the current gain?

 

Many thanks,

 

Bin

Outcomes