AnsweredAssumed Answered

UART PIN CONFIGURATION of ADSP-BF707

Question asked by Chiranjeev on Jan 27, 2017
Latest reply on Feb 1, 2017 by Jithul_Janardhanan

I am trying to locate the pin location of Tx, Rx, GND of UART0 in ADSP_BF707 to connect via jumper wires. As per the documentation the UART0_Tx and UART0_Rx are assigned the PIN_name PB_08 and PB_09. 

 

Also, the jumper wire connection pin are given as below

  

 

Can someone help me out in locating the pins Tx, Rx, CLK and Gnd for UART connection in the BLIP2  board?? 

 

Thanks and Regards

Chiranjeev

Outcomes