AnsweredAssumed Answered

Level Translation for clock

Question asked by amit.kn on Sep 14, 2011
Latest reply on Sep 15, 2011 by amit.kn

Dear Sir,

I am using virtex6 processor in my project which can support maximum 2.5V . I want to give a clock signal of 20Mhz to FPGA but my crystal voltage is 3.3V.So, i want to use a level translator btween FPGA and crystal.I have selected two IC's ADG3241 and ADG3231.So i want to know whether these device is suitable for my application, will it support clock frequency of 20MHz.As i am using crysal frequency as a sampling clock so it should be very accurate.

 

Please suggest me.

Thanks

Amit Kumar

Outcomes