AnsweredAssumed Answered

Interfacing HMC900 to HMC1197

Question asked by inavsystems on Jan 24, 2017
Latest reply on Feb 15, 2017 by DonY

I am using the HMC900 as a low pass filter before inputting the signal into the HMC1197.  The common mode voltage of the two devices is not compatible.  The minimum common mode voltage output from the HMC900 is 1.5V (5V/2 -1), but the HMC1197 requires 0.45V common mode voltage.  Is there a recommended way to shift the common mode voltage between the two devices. 

Outcomes