AnsweredAssumed Answered

Chip for 4k video decoding

Question asked by harshad on Jan 23, 2017
Latest reply on Jan 23, 2017 by GuenterL

Hi All, 

 

I have an application that requires 4k video decoding. I came across the chip ADV7619. I have one question. The HDMI 1.4 standards suggests input video support up to 4096 X 2160 @ 24Hz. The datasheet of the chip mentions 3840 × 2160 @ 30 Hz as the maximum display resolution supported. So my question is would the chip work if the input is 4096 X 2160 @ 24Hz. Would the output be distorted ? Or would the chip simply output 3840 × 2160 resolution video ?

Any help would be highly appreciated.  
 

Thanks, 

Srivats Iyer

Outcomes