AnsweredAssumed Answered

AD8676 Voltage phase reversal

Question asked by Tarzan on Jan 23, 2017
Latest reply on Feb 1, 2017 by Tarzan

I have a question about AD8676.
http://www.analog.com/media/en/technical-documentation/data-sheets/AD8676.pdf
#1, Does AD8676 will occur "phase reversal" when the input voltage exceed input common mode range?
Some data sheet say "No phase reversal ", But this datasheet is not mentined.

Just in case, We are using this device under the following condition:
G=1(Non-Inverting),Power supply=±5V(input common range =±3)

#2,
Is it possible to use SPICE simulation to see "phase reversal"?

]

Best regards,
Tarzan

Outcomes