AnsweredAssumed Answered

AD9361 Phase Calibration

Question asked by jom on Jan 21, 2017
Latest reply on Jan 23, 2017 by mhennerich

I'd like to know the hardware set-up procedure to run a phase cal on the AD9361.  Is there a Wiki for this as I could not find one.  I've had some response but I'm not certain whether it is working correctly.

 

I've tried everything from no inputs to looping the TX to the RX.  The latter gives me an error and the former just sets the "slide bar" to 360 (in the FMCOMM5 advanced tab).  I do get some nominal value but I have to set up a Transmit/DDS "One CW Tone" to one of the TX outputs for this to work.

 

These seems to be a lack of documentation on this...other than just reading the C code...which is a bit hard to follow for a non-programmer.

 

Thanks

 

I'm using the FMCOMMS5 with the ZC706.

Outcomes