AnsweredAssumed Answered

After migrating a BlackFin BF536 project from VisualDSP 4.5 to 5.1.2 the ldr intel hex file does not boot.

Question asked by falk on Jan 20, 2017
Latest reply on Sep 18, 2017 by Jithul_Janardhanan

Hi,

After migrating a BlackFin BF536 project from VisualDSP 4.5 to 5.1.2 raises following problem.

When I compile migrated source to create a .ldr file (intel hex format), burn it into SPI eprom, it will not boot properly.

- Loading old *.ldr file from before migration works fine
- 5.1.2 with HPUSB-ICE in debug works fine
- 5.1.2 with HPUSB-ICE in release works fine
So the hardware is fine, since it runs from the emulator pod as well as an older compilation in a boot prom.

 
best regards,

Falk

Outcomes