AnsweredAssumed Answered

Question about Building ADV7511 Xilinx Evaluation Boards Reference Design

Question asked by zed——cui on Jan 18, 2017
Latest reply on Jan 19, 2017 by zed——cui

hello everyone,

 

I am working with the "ADV7511 Xilinx Evaluation Boards Reference Design", with

"Win10 + Vivado 2016.2 + hdl_2016_r2 + no-OS-2016_R2" for ZedBoard. The problems which I met was very strange.

 

After building all the libraries (including: axi_clkgen; axi_hdmi_tx; axi_i2s_adi; axi_spdif_tx and util_i2c_mixer), I run the script:  "source ./system_project.tcl", The script created a board design in IPI, generate all the IP targets, synthesize the netlist and implementation. 

 

After that, I used "../adv7511_zed.sdk/system_top.hdf" to establish a new hardware project in Xilinx SDK, when I import the source files from the no-OS-2016_R2 and click "Refresh" button, one error occured:

 

cf_hdmi.h

"XPAP_AXI_SPDIF_TX_CORE_BASEADDR" undeclared(first use in this function)

 

It seems that the "XPAP_AXI_SPDIF_TX_CORE_BASEADDR" should be defined in "xparameters.h" , which should be generated automatically. But not for my program!!!

 

I also checked the "system.hdf" in hardware, and the Base Addr and High Addr were not assigend for axi_spdif_tx, I did not know if  this is the reason that "xparameters.h" did not define the "XPAP_AXI_SPDIF_TX_CORE_BASEADDR".

 

Can anyone help ?

Outcomes