AnsweredAssumed Answered

ADUM1401

Question asked by yka Employee on Jan 17, 2017
Latest reply on Jan 19, 2017 by yka

Hi,

 

Please see customer circuit attached:

SP_3_3V is UP before 3.3VA.

During this time NW_ISO_56N_PS1_OFFLINE_FPGA (pin 6) is driven High (which in turn switches OFF main power supply controlled through NW_ISO_56N_PS1_OFFLINE_FPGA signal) .

This is undesirable. So they shorted pins 6 and 7. This solves the problem. But due to this, the changes on pin 11 are not reflected on pin 6.

Basically, They are looking at option/solution to insure pin 6 remains low or High Z where +3.3VA is not up.  +3.3VA is up after 1-2 seconds after SP_3_3V.

 

Outcomes