AnsweredAssumed Answered

Serial SPI flash programming in BF-547

Question asked by Gana1970 on Jan 17, 2017
Latest reply on Feb 27, 2017 by Kader.M

Does ICE-1000 allow to program SPI serial flash using the VisualDSP++ 5.1.2 tool?

 

I have a custom board using BF-547 and serial SPI flash "AT45DB641E". I use ICE-1000 via the JTAG port for debugging currently. I want to use the SPI PROM attached to the DSP. I have created the appropriate loader file using the tool. However, when I try to program the device, I am unable to get the driver file for the SPI flash. I used the driver given in the Examples of the tool, and I am getting the following error message.

 

Is there any other tool, either in command line or in the GUI tool to download the loader file ?

 

Regards

Ganesan

 

PS: I am attaching schematics for the connection between DSP and Serial Flash.

 

VisualDSP error message

Outcomes