AnsweredAssumed Answered

Amplifying 100Mhz up to 5Vpp with LOW distortion

Question asked by Dexter on Sep 12, 2011
Latest reply on Sep 23, 2011 by JohnA

Hello,

 

I need to amplify an sinewave (1MHz-100MHz) up to 5Vpp with verry low distortion ( -90dBc). But i can not find an amplifier that can do this. Can somebody tell me if this is posible?

 

Frequency range     : 1MHz to 100MHz

Input Voltage           : 1Vpp

Output Voltage        : 5Vpp

Distortion                : -90dBc (or better) over the frequence range

Power cunsumption : Not verry importand ( <10W)

Rload                     : 100 Ohm

 

Construction like putting amplifiers paralel to distrubute the load form better distortion ar an option

 

Thanks in advance for any reaction

 

Ronald Dekker

Outcomes