AnsweredAssumed Answered

Can a SSM2305 be used as a single ended output amplifier with an external LC output filter?

Question asked by telcoeng on Jan 15, 2017
Latest reply on Jan 20, 2017 by Rajeev

I'm after a small amplifier to create an adjustable analog voltage with some drive current for a measuring application. If I use and DAC to drive the input then could one of the output pins be used as a pwm version of this signal. Then I'd have a low loss programmable supply.

Does the SSM2305 performance extend all the way to DC or is there a lower frequency limit? The datasheet charts stop at 20Hz but I did not find a lower frequency limit specification.

Outcomes