AnsweredAssumed Answered

ADM1278 ADISimpower Question

Question asked by JackH on Jan 15, 2017
Latest reply on Jan 16, 2017 by Marcus

Dear All:

I have some ADM1278 ADISimpower excel file parameter setting question.thanks

 

Q1: System specification's Rpowerup : if this register setting 100ohm or 1K ohm for the system will have any effect

 

Q2:Current limit Settings: Min/Max DC & Min/Max Reg. The DC& Reg what's the difference?. If my system continuous power:50A,which one should I use as a standard setting?

 

Q3:The ADM1278 have ISTART setting. How do I test it? my system setting ISTART:50A, power on continuous power:50A,IMax:60A, have any documentation refer? 

 

Best Regards,
Jack

Outcomes