AnsweredAssumed Answered

Is the highest isolation SPDT RF Switch in 3-6 GHz range the ADRF5021? (65 dB at 5 GHz)

Question asked by ibutter on Jan 10, 2017
Latest reply on Jan 13, 2017 by s.ilke
Needed specs
Frequency range: 3 - 6 GHz
Insertion loss < 3 dB
Isolation RFc to RF1 & RF2 > 60 dB at 3 - 6 GHz
Switching speed can be very slow, i.e. in the order of seconds.. My application isn't very standard!
Any advice welcome. I wondered if there's a left-field solution given I don't need fast switching..
Thanks,
Ian

Outcomes