AnsweredAssumed Answered

ADT7310 continuous read mode

Question asked by tmw on Jan 10, 2017
Latest reply on Jan 12, 2017 by Lluis

 

The datasheet states in continuous read mode, the temperature value register cannot be read when a conversion is taking place. If an attempt is made to read the temperature value register while a conversion is taking place, then all 0s are read. This is because the continuous read mode blocks read access to temperature value register during a conversion. 

 

Is it permissible to operate the ADT310 in continuous read mode (command = 0x54) while the device operation mode is continuous conversion (Configuration register bit [6:5] =00?  Will this result in all 0s being read at times?

Outcomes