AnsweredAssumed Answered

RGB input to ADV7280, instead of YPbPr

Question asked by Gortu on Jan 9, 2017
Latest reply on Jan 13, 2017 by JeyasudhaMuthuPerumal

I've just discovered beautifully low-pin ADV7280 – only 32 pins. However in datasheet there is no mention about component RGB, only about component YPbPr. What are chances that my SCART-only VHS player will not work with ADV7280 because of using apparently standard RGB, and not non-standard YPbPr, on the component pins of its SCART connector?

 

Maybe ADV7280 can be configured to expect R, G, B component?

 

PS. My VCR is Orion VH-2905.

 

Best regards,

Sebastian

Outcomes