AnsweredAssumed Answered

EVAL-ADAS1000SDZ test problem

Question asked by Jambo on Jan 9, 2017
Latest reply on Jan 31, 2017 by CatherineR

I have a EVAL-ADAS1000SDZ test problem,if add ECG specification dc offset 300mV ,the s waveform is truncated. is there a good suggestion?

 

Test Electrode:RA

Data Rate:2 kHz

Data Format:electrode

CH Config:Single Ended Input

GAIN:1.4

High Performance:2Msps Low Noise

Los Pass Filiter:150Hz

Attachments

Outcomes