stevereine

No OS example code and common.c file for zc706

Discussion created by stevereine Employee on Jan 8, 2017
Latest reply on Feb 10, 2017 by gverma

I have a customer using the AD9371, No OS, on the ZC706 platform. He's looking for an example of a common.c file, is frustrated overall because there does not seem to be any example code available, no examples folder in the API .zip file.

 

This is direct from the customer;

 

Problem is that the  No-OS API download does not contain an examples folder.

I understand that this and other files like common.c are to be customized for my custom target platform, but I am not there yet. I need to start with the a working platform which is the ZC706 ADVR9371reference platform. So if there was any code at all that works with the reference platform it would save a LOT of time and false starts trying to figure out how to get everything working from the ground up. That's one of the main purposes of a reference design, the other being for evaluation, which the TES application and IO Scope applications along with others provide nicely.

 

thanks...................Steve

Attachments

Outcomes