AnsweredAssumed Answered

Runtime Error in uart blocking-mode write

Question asked by abhiydv1793 on Jan 5, 2017
Latest reply on Mar 2, 2017 by Kader.M

Hello Sir/Madam,  I am using CCES 2.0.0 with BF548 EZ-KIT LITE. I am trying to write on the UART in blocking mode as given in the CCES example code. The code is build successfully, but at run time, an exception is thrown saying:  A non-recoverable error or exception has occurred.   Description:   A data CPLB miss has occurred without a corresponding CPLB  entry.   General Type:  RunTimeError   Specific Type: DCPLBMissWithoutReplacement   Error PC:      0xffa02bfc  I tried debugging the code and found out that the error comes inside the adi_uart_open() function while registering the "UART driver status interrupt handler". I am writing on UART1 with the exact settings as given in example sketch code for BF548. The project has only the following add-ins:  -> Pin multiplexing -> Startup Code/LDF -> UART Driver for Blackfin  I am new to CCES so it would be a great help if you can help me out of this problem. I hope to hear very soon from you. 
Abhishek Yadav

Outcomes