AnsweredAssumed Answered

Setting ADC Clk,R2/1 CLk, Clf RF in FCOMMS2 board

Question asked by SDontula on Jan 4, 2017
Latest reply on Jan 5, 2017 by sripad

How can I set the values of the ADC Clock, R1/R2 Clock, ClkRF and RSamp CLK in the FCOMMS2 platform. Do I need to upload a specific file. If so, can you please provide it. I would like to use ADC Clk as 368.64MHz, R2Clk = 122.88MHz, R1 Clk=61.44MHz, ClkRF=30.72MHz, Rsamp CLk=30.72MHz. I would like to use this scenario to measure the noise figure measurement as one of my other colleague measured an improved EVM under these settings. However he was using a legacy board and I am trying to use FCOMMS2 board and it is not clear form the GUI. Please help

Outcomes