AnsweredAssumed Answered

Supporting display resolution of ADV7630

Question asked by Se-woong on Dec 29, 2016
Latest reply on Jan 2, 2017 by JeyasudhaMuthuPerumal

Hello,

 

My customer asks some questions about a supporting display resolution of ADV7630.

" The ADV7630 incorporates a 1:2 HDMI splitter with 4:1 multiplexed input receiver that supports all mandatory and many optional 3D formats, DTV formats up to 1080p, and all  display resolutions up to UXGA (1600 × 1200 at 60 Hz)."

As your datasheet , ADV7630 seems to be able to suport that a maximum display resolution is 1600x1200 at 60Hz only.

And they should manage a 1920x1080 at 60Hz display resolution.

 

Could ADV7630 support 1920x1080 at 60HZ(FHD)?

And would you provide a list with all supporting display resolution of ADV7630 to them?

 

Regards,

Se-woong

Outcomes