Aaronwu

tftp not working on bf526 customer board

Discussion created by Aaronwu Employee on Sep 7, 2011
Latest reply on Oct 11, 2011 by Aaronwu

I am testing uboot loader compiled for  BF526 custom kit. It is  connected to a host PC(ip:10.7.143.34) running  aftpd daemon. It has  uImage stored in /tftpboot directory. The host m/c  tftpd is tested working with BF526-ezbrd from ADI.

In the custom bf526 board, Uboot comes up with the bfin prompt. I  tried running tftpboot on uboot prompt :

bfin > tftptboot 0x1000000 uImage

I get the following response on console:

****************************                                                       
Link up   detected                                                                                                                                                                                     
Using bfin_mac  device                                                                                                
TFTP from server 10.7.143.34; our IP address is  10.7.143.88                                                         
Filename 'uImage'.                                                                             
Load address:  0x1000000                                                                                              
Loading: T T T T  

*****************************

File transfer does not start at all. What could be the issue.

(P.S - Phy chip used on-board is RTL 8201(CP). It uses MII. I have  disabled RMII in my board config. Is there any other configuration for  using MII interface.)

Regards

Mala

Outcomes