AnsweredAssumed Answered

is the ucFS able to support the eMMC card on RSI  ?

Question asked by dell-jin Employee on Dec 26, 2016
Latest reply on Jan 13, 2017 by Kader.M

Hello all:

    the bf607 processor's RSI interface can support the eMMC card. the description in datasheet of BF607 is "Support for eMMC 4.3 embedded NAND flash devices", and the customer wants to use the ucFileSystem, we find the below in the release note of ucFS:  

   ADSP-BF606, ADSP-BF607, ADSP-BF608, ADSP-BF609
               o Devices supported: RAM Disk, SD Card, USB Mass Storage

 

so is the ucFS able to support the eMMC card on RSI  ?  or it must be a SD Card if using this filesystem.

Outcomes