AnsweredAssumed Answered

could not open source file

Question asked by Yane.Coceski on Sep 7, 2011
Latest reply on Sep 7, 2011 by CraigG

Hi guys,

 

I have a project that used to compile fine until about a week ago, i had to re format my computer and since then the project doesnt compile even though i backed up all of the files.

 

I get the following error when I try and compile the project

.\DSP_Based_Spectrum_Analyzer_basiccrt.s
.\adi_ac97.c
".\adi_ac97.c", line 25: cc0005:  fatal error: could not open source file
          "drivers/codec/adi_ac97.h"
  #include <drivers/codec/adi_ac97.h>     /* AC'97 driver includes    */
                                                                        ^

 

1 catastrophic error detected in the compilation of ".\adi_ac97.c".
Compilation terminated.
cc3089: fatal error: Compilation failed
Tool failed with exit/exception code: 1.
Build was unsuccessful.

 

I have attatched the whole folder of the project can someone please have a look at it and see where I have gone wrong

 

Thanks in advance

Attachments

Outcomes