AnsweredAssumed Answered

HMC6301 bandwidth registry settings

Question asked by Nutan on Dec 20, 2016
Latest reply on Dec 21, 2016 by Mark_D

Hi Mark

Mark_D

 

The receiver operates from 57 GHz to 64 GHz with up to 1.8 GHz of double-sided modulation BW. Does this mean the receiver contains filters to make the bandwidth configurable? If so can you please share the registry settings to receive a 500MHz signal centered around 58GHz and 63GHz?

 

In table8 - row5 the signal function says "Controls IF filter alignment in the RF mixer;ROW5<3:0> = 1111 for normal operation". What does normal operation means here?

 

Thanks

Nutan

Outcomes