AnsweredAssumed Answered

BF561 "video in video out" sample doesn't work

Question asked by Hoagn on Sep 7, 2011
Latest reply on Sep 8, 2011 by CraigG

Hello,

 

I'm using the AD561 EZ-KIT and want to try out the "video in video out"-sample of the Blackfin SDK vers. 4.10.

 

This is the camera is use: http://www.chinahtp.hk/ProductHtml/Product20014139.htm. It's a PAL-color camera, 'cause I'm from germany.In addition i use this monitor: http://www.pollin.de/shop/downloads/D600083B.PDF.

 

I connected the things via Jumper6, as descirbed in the readme and set the "#define   PAL_FRAME"-macro.

 

Some additional data:
- dsp_using: ADSP-BF56x
- Platform : ADSP-BF561 EZ-KIT Lite
- Emulator: ADDS-HPUSB-ICE

- Board rev.: 2.1
- BOM: 2.7
- VisualDSP++ vers.: Update 9.1


All  the switches are set as described in the readme and the PAL frame macro  is set. But there's nothing but a blue screen. I debugged the program and it seems on line 1289 of adi_pwr.c (switch (cmd->kind)) it jumps to a undefined exception. What can I do to solve this problem?


Regards, Sebastian

Outcomes