AnsweredAssumed Answered

AD9371 Triggering

Question asked by andrew.feldman on Dec 17, 2016
Latest reply on Dec 27, 2016 by gverma

Hello,

 

I am working with the Mykonos Transceiver Evaluation Board. I am feeding Tx1 back to ObsRx1 and Tx2 back to ObsRx2. I would like Tx1/2 and ObsRx1/2 to be connected to the same trigger signal - I do not need all four to be perfectly synchronized, I just need there to be a consistent delay between them, which I can measure and correct in post-processing.

 

I do not see an option to do this in the AD9371 TES or in Mykonos API documentation. Is there a way to configure this behavior, which I missed?

 

Best,

Andy

Outcomes