gverma

Issue with AD9371 uboot and kernel image load

Discussion created by gverma Employee on Dec 14, 2016

If you are facing errors while booting the Linux kernel shipped along with SD card, follow these steps to correctly set uboot.

  • Connect a USB mini cable between your computer and the ZC706 board UART port
  • Open a Tera Term window (or equivalent tool) and connect to the proper UART port
  • Turn on the ZC706 board and stop the autoboot when prompted
  • Enter the following command:  env default –a
  • Enter the following command: saveenv
  • Enter the following command: reset

 

This process should ensure the ZC706 has the proper uboot loaded into the flash memory on the board. 

Outcomes