AnsweredAssumed Answered

Question for AD7730 Filter

Question asked by Jake01 on Dec 14, 2016
Latest reply on Dec 21, 2016 by Jake01

Hi

 

I'm testing AD7730 for weighscale application

From the datasheet, I could find Sinc3 and FIR filter.

FIR filter looks like good performance at 20Hz ~ 60hz noise rejection with slow settling.

S0, I tried to use Sinc3 Filter to reject noise at 20Hz ~ 60Hz.

 

Question :

1. It seems like Sinc3 Filter is not appropriate to reject noise at 20Hz ~ 60Hz. Am I right?

When I saw sinc filter of AD719x series, seems like it can reject 20Hz ~ 60Hz noise.

(Because of output data rate constraint) See the below!

2. Is it possible to apply oversampling technique for AD7730?

e.g) When I set the ODR to 200Hz, Output noise is bigger than 400Hz ODR.(Fast = 1, CHOP enabled)

If so, can you give me data to understand it?

 

3. If Sinc3 filter is not stand for rejection noise of 20Hz ~ 60Hz, What is its function?

Outcomes