AnsweredAssumed Answered

using AD8604  below -40°C

Question asked by hallodrius on Dec 12, 2016
Latest reply on Jan 17, 2017 by krisf

Hi, im using this OPAMP now for a long time and feel very well with the quality.
Now in have to use my special ciruit on temperatures up to -55°C/+55°C

I know, this OPAMP works well (ive tested up to -60°C),

but my request is for usage up to -55°C on the datasheet.

 

So i need a new OPAMP with this temperature-range, or message from AD "its save to use this in your condition"

 

 

sincerely

Anselm

 

p.S.: i need this very nice low offset & offsetdrift over temperature 2µV/°K

Outcomes