AnsweredAssumed Answered

EVAL-ADV8005 TX1

Question asked by qwerty78 on Dec 9, 2016
Latest reply on Dec 14, 2016 by JeyasudhaMuthuPerumal

I'm using the EVAL-ADV8005-SMZ and AVES to manually configure some registers.  After allowing the default firmware to initialize the registers I am able to see a video output from JT4.  If I toggle TX1 system_pd on and off without making any other changes, the output disappears from the monitor and does not return when the TX1 system is re-enabled. 

 

When the system_pd of TX1 is toggled, are there other registers that need to be updated in order to properly output the video?

Outcomes