AnsweredAssumed Answered

Boot Multi-dxe from Flash

Question asked by bachabharat on Dec 8, 2016
Latest reply on Dec 26, 2016 by Jithul_Janardhanan

I am using BF-609 EZ KIT with standalone agent. 

 

Previously in BF 537, I have flashed 2 dxe at offsets of 0x0000 and 0x20000. In the first application code I called the 2nd dxe which is at offset  0x20000 using Boot_dxe_flash (0xEF00 0008) with correspoding dxe2 flash address in R7 and worked fine.

 

I would like to do the same in 609 and have come across callable API rom_boot at 0xB800 000C with some parameters. I don't want to customize the default configuration using those parameters and also can't get some parameters like dBlockCount, pCallHook, dFlags. Is there any other function which i can call with the start address of boot stream or Can I pass all the other parameters as 0 or NULL.

 

My settings are as below

bcode 0x6

format binary.

 

Thanks and Regards,

Bharath

Outcomes