AnsweredAssumed Answered

AD9910 frequency sweep initial phase

Question asked by adr.mzg on Dec 8, 2016
Latest reply on Dec 8, 2016 by adr.mzg

Hello, I'm using an AD9910 DDS to generate a triangular frequency sweep continuausly, using the no-dwell mode. In order to test the acquisition system, I'm reading the output with a high speed ADC with SYNC_CLK as input clock and DROVER as acquisition trigger. Reading the datashet I expect that when the ramp reaches the low or the high limit, the phase accumulator clears, so that each sweep should start with a constant phase. However, when inspecting DROVER and the output, the phase seems to be different everytime (see attached oscilloscope captures, where blue is DROVER and yellow the output). Am I missing something? Thanks in advance!

Attachments

Outcomes