AnsweredAssumed Answered

The sampling rate of  AD9234-1000

Question asked by EasonLife on Dec 6, 2016
Latest reply on Dec 9, 2016 by UmeshJ

HI:

   I have a problem with AD9234-1000. It can be seen from the datesheet that the Chip_GRADE register is read-only. And we can see the range of clock rate of  AD9234-1000 is 0.3~4GHz.

   The question is : can I use the  AD9234-1000 in the 500sps sampling rate?

   Thanks!

Outcomes