AnsweredAssumed Answered

How to use ADP1051 in application with output voltage higher than 64V? In the datasheet of theADP1051 we can read that Vout command is limited at 64V whereas the voltage divider is external to the ADP1051.

Question asked by GB32 on Dec 5, 2016
Latest reply on Dec 5, 2016 by LtCommData

How to use ADP1051 in application with output voltage higher than 64V?

In the datasheet of theADP1051 we can read that Vout command is limited at 64V (Table 21) whereas the voltage divider is external to the ADP1051.

I need to drive a DC/DC with an output voltage of 110 to 130V, is-it possible?

 

Regards,

 

Guillaume Boulet

Outcomes