AnsweredAssumed Answered

ad9913

Question asked by gkrf on Nov 30, 2016
Latest reply on Aug 21, 2017 by gkrf

Hi, on the AD9913, how much worse should the phase noise be when the PLL is engaged (2x multiplication) vs.

when it is direct fed? In this specific case:

 

Fref: 90 MHz  = sysclk

vs.

Fref: 90MHz using PLL=2x, 180 MHz = sysclk

 

For a FIXED output frequency, would there be a 20*log(2) degradation? That is not clear to me since the output frequency

is actually fixed.

 

The data sheet does not show this kind of comparison, only residual phase noise for direct fed and absolute

phase noise for PLL=4x.

 

Thanks, Jerry

Outcomes