AnsweredAssumed Answered

HMC832 SPI Voltages

Question asked by MuhammadAliGhafoor on Nov 27, 2016
Latest reply on Nov 28, 2016 by dyoung1

SPI pins are logic CMOS inputs. Datasheets tells that the maximum voltage at logic inputs should not exceed 60 % of DVDD. If i use 3.3 V DVDD, would the device work properly with 3.3 V applied at SPI pins. Most of teh microcontrollers SPI interface work at 3.3 V, so I would like to operate the PLL SPI interface at 3.3 V. But datasheet says that it should not exceed 60% of 3.3 V (if 3.3V DVDD is used). 

 

Waiting for your feedback

 

Regards,

Ali Ghafoor,

RF System Engineer

Outcomes