AnsweredAssumed Answered

Switched Capacitor High Speed ADC Differential Input Resistance

Question asked by balajiyoki on Nov 24, 2016
Latest reply on Dec 1, 2016 by DougI

For AD9253-105 converter , can I consider the given differential input resistance for matching with a 50 ohm signal source? Given resistance value is 5.2 K ohm, if not what are the factors to be considered ?

 

My sampling rate is  102.4 MHz and input bandwidth of 40 MHz centered at 76.8 MHz for my application.

Outcomes