AnsweredAssumed Answered

ADSP-SC589 SD-Card boot problem

Question asked by jaro73 on Nov 23, 2016
Latest reply on Nov 24, 2016 by Aaronwu

I have a problem with booting linux from SD-Card.

Listing from u-boot command line:

 

sc # run sdboot
SF: Detected W25Q128BV with page size 256 Bytes, erase size 4 KiB, total 16 MiB
SF: 20480 bytes @ 0x900000 Read: OK
5667168 bytes read in 421 ms (12.8 MiB/s)
## Booting kernel from Legacy Image at c2000000 ...
   Image Name:   Linux-4.0.0-ADI-1.1.0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    5667104 Bytes = 5.4 MiB
   Load Address: c2008000
   Entry Point:  c2008000
   Verifying Checksum ... OK
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree

 

My u-boot version : U-Boot 2015.01 ADI-1.1.0 (May 30 2016 - 14:25:12)

Outcomes