AnsweredAssumed Answered

ADAU145x SAFELOAD word using SPI

Question asked by dbnsExpert on Nov 16, 2016
Latest reply on Feb 9, 2017 by DaveThib

Hello everybody,

 

About safeload registers:

They are 32 bits registers. So, if i using SPI to load 4 bytes (1 byte at a time), the increment will occur only when the 32bit is reached? 

The number of bytes to send are in bytes or words (sigma studio show it in bytes)?

Compiler can put the safeload registers in DM0 or DM1. When i write to one of the (DM0 or DM1) should i consider their address ? Or just safeload address?

Because DM0 and DM1 have their own address. Like the print below:

Attachments

Outcomes