AnsweredAssumed Answered

HMC703 HMC582 Circuit

Question asked by Sunzeyue on Nov 10, 2016
Latest reply on Nov 10, 2016 by Sunzeyue

Hi,

   I recently used the HMC703+hmc582 to generate 11.655GHz signal. It can be properly locked to 11.255GHz, but it cannot be locked when the frequency is above 11.56GHz.What are the reasons for this problem? And how to solve it? Thank you!

 

Register configuration

  01h=wr|a5~a0|d23~d0|X=0|000001|000001|0

  02h=wr|a5~a0|d23~d0|X=0|000010|000001|0

  03h=wr|a5~a0|d23~d0|X=0|000011|00001D|0

  04h=wr|a5~a0|d23~d0|X=0|000100|233333|0

  05h=wr|a5~a0|d23~d0|X=0|000101|654321|0

  06h=wr|a5~a0|d23~d0|X=0|000110|001D1E|0

  07h=wr|a5~a0|d23~d0|X=0|000111|004865|0

  08h=wr|a5~a0|d23~d0|X=0|001000|036FFF|0

  09h=wr|a5~a0|d23~d0|X=0|001001|747264|0

  0Ah=wr|a5~a0|d23~d0|X=0|001010|000000|0

  0Bh=wr|a5~a0|d23~d0|X=0|001011|01E061|0

  0Ch=wr|a5~a0|d23~d0|X=0|001100|000000|0

  0Dh=wr|a5~a0|d23~d0|X=0|001101|000000|0

  0Eh=wr|a5~a0|d23~d0|X=0|001110|000000|0

  0Fh=wr|a5~a0|d23~d0|X=0|001111|000001|0

 

Attachments

Outcomes