AnsweredAssumed Answered

ADAU1452's "Linear Gain", "Single Volume Control", "Mute"

Question asked by IRON on Nov 8, 2016
Latest reply on Nov 17, 2016 by DaveThib

Hello all,

I have a question on the SigmaStudio's modules.

 

I looked at the help page of "Linear Gain", "Single Volume Control", and "Mute".

Are they basically the same things?(their usage is to just change the parameter? then the volume changes?)

Are they internally calculating in the same way?

 

If the above is true, 

When implementing the "Mute" module, is it also possible to use the "Mute" module as if it is a "gain" module controlling from a master micro-controller in the system?

What I am asking is if the mute module can have 2 capabilities of both "mute" and "gain" (if the internal calculation is the same.) so that I do not have to implement 2 modules.

 

Best Regards,

Yuta M

Outcomes