AnsweredAssumed Answered

ADF9010 Question

Question asked by hello_itman on Nov 8, 2016
Latest reply on Nov 11, 2016 by pwalsh

reference clk is 10MHz,R counter=10, P=16,A counter=16,B counter=229.
have set Bit F5&F4(MUTE UNTIL LOCK DETECT) of control latch to "1" , The frequency of LO is 925MHz, meanwhile ,the tx signal is off and on alternately . but, when i set Bit F5&F4(MUTE UNTIL LOCK DETECT) of control latch to "0" , The frequency of LO is 930MHz, and the TX signal is normal. could you help me to solve this question?

Outcomes