AnsweredAssumed Answered

ADXRS290 temperature sensor

Question asked by M-Atwya on Nov 7, 2016
Latest reply on Nov 7, 2016 by NevadaMark
Branched to a new discussion

Hello,

 

I wanted to ask if the ADXRS290 temperature sensor measurements are used within the ADXRS290 for internal temperature compensation ?
I assume it is not used internally for temperature compensation. If my assumption is correct, would I be correct in assuming that the lack of tempearute compensation is a major contributor to the ADXRS +/- 9 Degrees/second Offset Error across TA= -20 to +60 °C?

 

I had a look at a similar quesiton on the forum but still didnt quite get the answer I was looking for ( "The use of ADXRS290 temperature sensor" ).
Many thanks.

Outcomes